AIN#.ZERO
Description
AIN#.ZERO causes the drive to zero the analog input signal (AIN#.VALUE). You may need to execute this command more than once to achieve zero offset.
-
- AIN#.OFFSET is modified in this process.
Examples
Code
--> AIN1.VALUE 0.056 V --> AIN1.OFFSET 0 V --> AIN1.ZERO --> AIN1.VALUE 0.000 V --> AIN1.OFFSET -0.056 V
Context
For more information see Analog Input.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Command |
| Units | N/A |
| Range | N/A |
| Default Value | N/A |
| Data Type | N/A |
| See Also | |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AIN1.ZERO |
3780h |
06h |
Unsigned32 |
- |
- |
Write only |
No |
|
AIN2.ZERO |
3781h |
06h |
Unsigned32 |
- |
- |
Write only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
23250 |
1 |
23250 (0x5ad2) |
AIN1.ZERO |
Unsigned8 |
Read/Write |
No |
|
23251 |
1 |
23251 (0x5ad3) |
AIN2.ZERO |
Unsigned8 |
Read/Write |
No |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AIN1.ZERO |
23250 |
Unsigned8 |
Read/Write |
- |
|
AIN2.ZERO |
23251 |
Unsigned8 |
Read/Write |
- |